Browse FAQs

Can we use the VW3G48101 keypad to download program and upload to an identical ATS48?

Published date: 28 January 2020

Issue :
Can the VW3G48101 remote keypad be used to download parameters from an old ATS48 to another ATS48?

Product Line :
Altistart 48, ATS48

Environment :
All

Cause :
Replacement soft starter

Resolution : 
No, the remote keypad is for an interface between the user and softstart only.  To transfer program use the software, SoMove with the Altistart DTM loaded.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.