Browse FAQs

Galaxy VX; How to configure the Network Communications options

Published date: 21 January 2020

Issue:
How to configure the Network Communications options for Galaxy VX



Product line:
Galaxy VX - all


Environment:
All


Cause:
How to set up network communications for the UPS


Resolution:
The network can be configured for the display and for the cards in Smart Slot 1 and
Smart Slot 2.

From the home screen on the display select Configuration > Network and
select either Display, Smart Slot 1, or Smart Slot 2 if present.

Configure the following settings:
TCP/IPv4: Enable IPv4 (if applicable), and select the Address Mode
(Manual, DCHP, or BOOTP).



TCP/IPv6: Enable IPv6 (if applicable), select Auto Configuration or
Manual Configuration, and select the DHCPv6 Mode (Router controlled,
Non-Address Information Only, Never, or Address and Other
Information).

NOTE: Tap Addresses to see all valid IPv6 addresses.



Web Access: Enable Web (if applicable) and select the Access Mode
(HTTP or HTTPS).
NOTE: Not available for Smart Slots.



FTP server: Enable FTP (if applicable).
NOTE: Not available for Smart Slots.