Browse FAQs

The images imported into EcoStruxure Augmented Operator Advisor Builder are in the wrong orientation.

Published date: 13 February 2020

Issue:
When importing an image taken in Portrait Mode into EcoStruxure Augmented Operator Advisor Builder, the resulting image will appear in Landscape Mode. This makes working with the image difficult as you have to look at the screen sideways when building your application.

Product Line:
EcoStruxure Augmented Operator Advisor

Resolution:
Currently the EcoStruxure Augmented Operator Advisor does not have a feature to allow a user to rotate the image to be in Portrait or Landscape mode. The image will come in as Landscape mode by default. However, the workaround is to edit the image with software such as Microsoft Paint to rotate the image before importing it into the builder.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.