Browse FAQs

Is the VW3A1103 compatible with the ATV600 & ATV900 drives?

Published date: 04 March 2020

Issue : 
Keypad accessory compatible with the Altivar Process drives?

Product Line :
Altivar Process ATV630, ATV930

Environment :
n/a

Cause :
Adding protection for door mounting purpose

Resolution : 
No. The VW3A1103 is not compatible with the Altivar Process drive. The ATV600 & ATV900 drive is already equipped with a keypad that is already IP65 rated and does not need the extra accessory.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.