Browse FAQs

What can cause EcoStruxure Control Expert to fail to launch and display the error "Instance of SecPBS or SecUBS Creation failed Opening them failed"

Published date: 27 February 2020

Issue:
Control Expert is failing to launch and displaying "Instance of SecPBS or SecUBS Creation failed Opening them failed"

Product Line:
EcoStruxure Control Expert, Unity Pro

Environment:
Windows 7, Windows 10, 32-bit, 64-bit

Resolution:
When the error "Instance of SecPBS or SecUBS Creation failed Opening them failed" is encountered, it is recommended to uninstall and reinstall EcoStruxure Control Expert / Unity Pro. This will remote a certain corrupted file and re-create it.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.