Browse FAQs

How do I customize Shortcut Keys in EcoStruxure Machine Expert?

Published date: 30 March 2020

Issue
I would like to customize or remap Keyboard Shortcuts in EcoStruxure Machine Expert. How is this done?

Product Line
EcoStruxure Machine Expert, SoMachine

Environment
PLC Configuration software suite for Windows

Resolution
To change or map new Keyboard Shortcuts, use the Tools -> Customize dialog, in the Keyboard tab.

Example Steps:
1. Choose the command Tools -> Customize.
⇒ The Customize dialog box opens.
2. Choose the Keyboard tab.

3. Select the category Find/Replace from the Categories list
⇒ All commands in this category are listed on the right.
4. Select the command Find/Replace -> Find
5. Click into the field Press shortcut keys.
6. Press Ctrl+Shift+F.
⇒ Machine Expert adds the key combination to the field.
7. Click Assign.
⇒ The keyboard shortcut is assigned to the command.
8. Click OK.


From this point in time, when you press the keyboard combination Ctrl+Shift+F, it will call the Find function within EcoStruxure Machine Expert.
    
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.