Browse FAQs

What are the main differences between Micrologic X and Micrologic 2/5/6/7 ?

Published date: 30 March 2021

Micrologic X control unit is designed and dedicated for MTZ range only. It is an advanced control unit and comes embedded with features such as Bluetooth, NFC and a USB-C port whereas Micrologic 2/5/6/7 didn’t have these features.
 
Micrologic 2/5/6/7Micrologic X
A, E, P, HX

Micrologic X is customizable through Digital Modules (can be purchased through GoDigital ).
It has EcoStruxure Power Device App smartphone app feature for easy operation and maintenance.
https://www.se.com/au/en/work/products/product-launch/ecostruxure-power-device/
It has a USB-C port and it uses EPC - EcoStruxure Power Commission software for testing, commissioning and reporting. 
https://www.se.com/au/en/work/products/product-launch/ecostruxure-power-commission/#Features%20and%20Benefits

Micrologic3.gif

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.