Browse FAQs

What is the angle of travel for the 22mm 2 and 3 position selector switches?

Published date: 04 March 2020

Issue:
22mm selector switch angle of travel

Product Line:
Harmony XB4 XB5 22mm selectors

Environment:
n/a

Resolution:
The angle of travel for the 2 position is 70 degrees and 3 position is 45 degrees.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.