Browse FAQs

How to install a control wire into a Masterpact NW/NT push in connector

Published date: 15 May 2020

Issue:
How to install a control wire into a Masterpact NW/NT push in connector

Product Line:
Masterpact NT and NW

Resolution:
Place a small flat screwdriver into the square hole (do not pry up or down), then insert control wire into the round hole just above the screwdriver. Then remove the screwdriver. The acceptable wire size is 22-14 AWG(.4-2.5mm^2). Strip length is .3 in. (8mm).

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.