Browse FAQs

What is the difference between a 9001KRD1U and 9001KR1U?

Published date: 24 August 2020

Issue:
Do 9001KRD1U and 9001KR1U function the same?

Product Line:
Push Buttons and Operator Interace  

Environment:
9001K Heavy Duty Specialty Operators

Resolution:
The 9001KR1U is a momentary operator for contacts to drop back to normal state immediately when the button is released.  The 9001KRD1U is a time delay operator that delays contact action back to normal state when the button is released.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.