Roll over image to zoom in

NSYTRAABV35
Grey surface treatment finishing
It is compatible with TRV screw terminal
spring terminals significantly reduce wiring time
spring terminals eliminate the need for regular re-tightening
Technology allows the connection of flexible conductors with or without cable ends
Environmental Data
Use Better
Packaging made with recycled cardboard
Yes
Use Again
Take-back
No