Men
Abrha Milaw 🇪🇹 2:07:05
Asefa Mengistu 🇪🇹 2:07:25
Paul Lonyangata 🇰🇪 2:07:29
Women
Gelete Burka 🇪🇹 2:22:47
Azmera Gebru 🇪🇹 2:22:52
Azmera Abreha 🇪🇹 2:23:35
Disabled athletes
Julien Casoli 🇫🇷 1:36:57
Heinz Frei 🇨🇭 1:45:37
Vitaliy Gritsenko 🇷🇺 1:46:35
Abrha Milaw 🇪🇹 2:07:05
Asefa Mengistu 🇪🇹 2:07:25
Paul Lonyangata 🇰🇪 2:07:29
Women
Gelete Burka 🇪🇹 2:22:47
Azmera Gebru 🇪🇹 2:22:52
Azmera Abreha 🇪🇹 2:23:35
Disabled athletes
Julien Casoli 🇫🇷 1:36:57
Heinz Frei 🇨🇭 1:45:37
Vitaliy Gritsenko 🇷🇺 1:46:35
Our new personal best: 0 carbon
For the seventh straight year Schneider Electric proudly sponsored the Marathon de Paris. When our commitment to offset the Paris Marathon’s carbon footprint kicked off in 2016, we compensated 50% of the event’s emissions. This year – just four editions later – we have achieved 100%.

Join the #SEGreenRunners
The race for sustainability doesn’t end on April 14. Join the #SEGreenRunners community and sustain the pace throughout the year.
Het Livelihoods Hifadhi-project in cijfers
50.000
hectaren bosgebied minder in Kenia, elk jaar
150.000
kooktoestellen zullen verkocht zijn van 2013-2022
$2
is de prijs van één kookfornuis
60%
vermindering in houtgebruik, vergeleken met de traditionele kachel
13.000
ton hout zal men besparen door het project, in 10 jaar
1 miljoen
ton CO₂ minder is de totale doelstelling van het project