Populaire vragen (FAQ's) zoeken
Safety limit switches XCS Atex - Are the XCSDMC79*EX or XCSDMC59*EX magnetic switches UL & CSA approved
The magnetic switches XCSDMC79*EX or XCSDMC59*EX are Atex certified by the Ineris certified body according to the european Atex directive 2014/34/EU and the relevant EN standards. They are not UL or CSA certified because the rules are not harmonized in North America. Attached Atex essential guide extract showing the certification of these switches.
Gepubliceerd voor:Schneider Electric Belgium
bijlage(n)
Ontdek meer
Ontdek meer