{}

Populaire vragen (FAQ's) zoeken

{"searchBar":{"inputPlaceholder":"Op trefwoord zoeken of een vraag stellen","searchBtn":"Zoeken","error":"Voer een trefwoord in om te zoeken"}}

Which control box (HMIGTU) can be used with the HMIGT752 or HMIDT952 and Somachine software?

Issue:
Which control box (HMIGTU) can be used with the HMIDT752 or HMIDT952 and Somachine software?

Product Line:
Somachine, HMIG3U, HMIG5U, HMIG5U2, HMIDT752, HMIDT952

Resolution:
The HMIDT752 and HMIDT952 will only support the HMIG5U2 control box and requires Somachine v4.3 Patch 2 and SP6.1 for Vijeo Designer v6.2 or higher.

Bent u geholpen met deze informatie ?

Ontdek meer
Productfamilie
Vijeo Designer
Ontdek meer
Productfamilie
Vijeo Designer