{}

Populaire vragen (FAQ's) zoeken

{"searchBar":{"inputPlaceholder":"Op trefwoord zoeken of een vraag stellen","searchBtn":"Zoeken","error":"Voer een trefwoord in om te zoeken"}}

Why am I getting an error when trying to import tags from RSLogix5000 into Vijeo Designer using the Link Variables feature with add on instructions?

Issue

Why am I getting an error when trying to import tags from RSLogix5000 into Vijeo Designer using the Link Variables feature with add on instructions?

Product Line

Vijeo Designer, Magelis HMI

Environment

Configuration software in Windows PC

Resolution

If some variables' add on instructions comment length is more than 256 characters, it will save as an error, so when Vijeo Designer tries to import the tags, it will popup as an error.

You can delete some comment content if comments' length is more than 256 in a L5K file.
Once the add on instructions are less than 256 in length, reimport the new L5K file.

Bent u geholpen met deze informatie ?

Ontdek meer
Productfamilie
Vijeo Designer
Ontdek meer
Productfamilie
Vijeo Designer