Brasil

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.

Pode selecionar outro país para consultar os produtos disponíveis ou aceder ao nosso website global para obter informações sobre a empresa.

Escolha outro país ou região

  • Operators in power station control room working with technical challenges, sustainability reporting.

    Automated fault detection and Diagnostics

  • Read

    • Read more about Schneider Electric solutions

      Building Analytics Brochure

      Building Analytics gives you the ability to optimize operations by making fact-based imrovements taht are proven to lower energy costs, extend equipment life, and improve tenant comfort, making a positive and measurrable impact on your bottom line. Download the brochure to learn more
    • Read more about Schneider Electric solutions

      Building Analytics Managed Service Handout

      Building Analytics is an advanced life cycle managed service that provides hosted technology and remote monitoring services to deliver advanced building diagnostics and operational improvement opportunities. Download the handout to learn more
    • Read more about Schneider Electric solutions

      Optimizing Buildings Using Analytics and Engineering Expertise

      Building Management Systems (BMS) offer facility managers many advantages. Leveraging BMS data through analytic software and combining it with expert engineering services creates actionable intelligence that can reduce energy costs by up to 30%. Download the white paper to read more
    • Read more about Schneider Electric solutions

      Guideform Specification: Automated Monitoring Based Commissioning Section [25 08 01] [13811]

      AUTOMATED MONITORING BASED COMMISSIONING SYSTEMS
      Scope: Provide labor, material, equipment, related services, and supervision required, including, but not limited to, manufacturing, fabrication, erection, and installation for automated monitoring based commissioning (AMBCx) systems as required for the complete performance of the work, and as shown on the Drawings and as herein specified.
      The work specified in this includes, but shall not be limited to, the following:
      1. The AMBCx provider shall ensure that data sufficiency conditions of this Section are met. This shall require coordination with the Energy Monitoring and Control Systems (EMCS) Contractor (if different). 
      2. The requirements of this Section apply to all EMCS elements of [Division 25 - IntegratedAutomation] [Section 13800 - Building Automation and Control].
      Read more: Guideform Specification: Automated Monitoring Based Commissioning Section [25 08 01] [13811]
    • Read more about Schneider Electric solutions

      Schneider Electric Seneca Plant

      Leading by example to eliminate energy waste, the company’s manufacturing facility in Seneca, South Carolina used Schneider Electric Building Analytics managed service to fine-tune its operations while reaping the energy-saving benefits. Case Study: Schneider Electric Seneca Plant
    • Read more about Schneider Electric solutions

      City of Henderson: Part of SmartStruxure™ solution, Building Analytics provides automated fault detection and diagnostics for forecasted energy and cost savings

      The US City of Henderson, Nevada, is nestled among three of the most renowned manmade attractions – the neon of Las Vegas, the engineering marvel of Hoover Dam, and the tranquil beauty of Lake Mead. One of the younger cities in the Southwest, Henderson’s infrastructure has grown efficiently over the past 20 years due to the efforts of private citizens and city leaders working together to build a community that is conducive to business, the entrepreneurial spirit, and a high quality of life for its over quarter-million residents. Case Study: City of Henderson: Part of SmartStruxure™ solution, Building Analytics provides automated fault detection and diagnostics for forecasted energy and cost savings
    • Read more about Schneider Electric solutions

      Fault detection in a research laboratory ventilation system

      In the fall of 2010, monitoring services were provided for a 450,000 square-foot research laboratory in the greater Boston area. The five-year-old facility was equipped with state-of-the-art energy efficient HVAC systems, including 10 ventilation units with capacity exceeding 50,000 CFM and several hundred variable air volume (VAV) boxes, to serve a mix of laboratory, office, and educational space. Building Analytics provides facility teams with continuous system fault detection to automatically evaluate and organize the condition of equipment. This information enables proactive building maintenance while ensuring persistent energy efficiency, which could result in significant ongoing energy and cost savings. Case Study: Fault detection in a research laboratory ventilation system
    • Read more about Schneider Electric solutions

      Commissioning rooftop units in a community center

      Building Analytics diagnostics and reporting were deployed to provide ongoing commissioning on newly installed rooftop units at a one-story community center housing offices, a gymnasium, and community rooms. Five RTUs were connected to the cloud-based system for monitoring and diagnostics. Almost immediately, several problems with RTU scheduling, compressor cycling, and simultaneous heating and cooling demands were found leading to controls adjustments to reduce energy consumption and costs. Case Study: Commissioning rooftop units in a community center
    • Read more about Schneider Electric solutions

      Facilitating utility incentives: Monitoring and verification at a multi-tenant office tower

      This multi-tenant office building deployed Building Analytics diagnostics and reporting to help discover efficiency opportunities, and to facilitate participation in the Massachusetts Pay for Performance (P4P) utility incentive program. Building Analytics diagnostics were used on the central air handlers, chilled water loop, and hot water loop. The building’s management committed to six low-cost energy conservation measures (ECM) for pre-ECM and post-ECM monitoring in order to prove the energy savings targeted in their P4P project application. Other equipment issues found by Building Analytics diagnostics are being corrected as they occur. Case Study: Facilitating utility incentives: Monitoring and verification at a multi-tenant office tower
  • Learn

    Análise de Edifício


    Veja como obter resultados para melhorar a eficiência energética e operacional. Faça o download do Infográfico
  • Watch

    • Unlock Your Super Hero Vision

      Building Analytics gives you the superhero ability to see hidden optimization opportunities.