Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.

Pode selecionar outro país para consultar os produtos disponíveis ou aceder ao nosso website global para obter informações sobre a empresa.

Escolha outro país ou região

  • Default Alternative Text
    for Low-Voltage and Medium-Voltage Applications

    Direct Replacement Circuit Breakers

    • Solutions

      Direct replacement modernization solutions feature new circuit breakers designed to fit into the existing cubicle with little-to-no modification to the switchgear cell. A direct replacement solution reduces downtime since there is minimal (if any) outage on the equipment bus.

      Low-Voltage Direct Replacement Circuit Breakers
      A standard Masterpact cradle is installed into an adapter cradle to form one assembly, which is then installed into the switchgear cubicle. This cradle-in-cradle assembly locks into place and remains in the switchgear cell after the initial installation. The new Masterpact circuit breaker racks in and out of the adapter cradle. A new door is installed, however cell interlocks, the racking mechanism and the switchgear structure are not modified.

      Medium-Voltage Direct Replacement Circuit Breakers
      Designed to fit into an existing switchgear cell without modification, Magnum circuit breakers will correctly interface with the existing compartment cell and maintain safety interlocks built-in the original equipment design.
    • Differentiation

      Our cost-effective modernization solutions will upgrade your electrical system to current technology. Downtime is minimized when compared with the demolition and replacement of existing equipment.

    Benefits

    • Default Alternative Text

      Our Masterpact NT/NW low-voltage circuit breakers provide solid state protection, reduce the potential for an arc flash event and do not require maintenance under normal operating conditions. 

      Reduced costs and less downtime for equipment upgrades compared to new switchgear installation 

      Cost-effective electrical system upgrade

      Maintains electrical system integrity during upgrade 

      Eliminates the need for obsolete or unavailable spare parts 

      Features a one-year equipment warranty

    • Default Alternative Text

      Magnum medium-voltage direct replacement circuit breakers will rack into the switchgear line-up and correctly interface with the existing compartment cell. The original racking mechanism, safety interlocks and the primary/secondary disconnects are maintained and the switchgear structure is not modified. 

      Reduced costs and less downtime for equipment upgrades versus new equipment 

      Enhanced equipment reliability 

      Maintenance free vacuum and SF6 bottles

      Available for most manufacturers’ equipment 

      Complete factory testing, backed by standard equipment warranty 

      ANSI & IEEE designs with complete documentation 

      Upgraded MVA ratings and nuclear certification available upon request