Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Image of General Specification for Intelligent Motor Protection Relay

General Specification for Intelligent Motor Protection Relay

This specification defines the Requirements for the Intelligent Motor Protection Relay performing Metering, Monitoring and Motor Protection functions, associated with User Interface and communication features.

Date: Nov 01 2016 | Type: Specification guide
Languages: English | Version: 1.0
Document Number: int_motor_relay_specification

Files

File Name
intelligent_motor_protection_relay_spec_en_V8_2015_10_22.docx