Issue:
What enclosures are available for the M frame PowerPact circuit breakers?
Product Line:
Circuit Breaker Enclosure
Environment:
PowerPact M frame Enclosure
Resolution:
The available enclosures for the M PowerPact circuit breaker include:
M800S - NEMA Type 1
M800R - NEMA Type 3R
M800DS - NEMA Type 4/4X/5. Type 304 Stainless Steel
M800SS - NEMA Type 4/4X/5 Type 316 Stainless Steel
M800AWK - NEMA Type 12/3R
What enclosures are available for the M frame PowerPact circuit breakers?
Product Line:
Circuit Breaker Enclosure
Environment:
PowerPact M frame Enclosure
Resolution:
The available enclosures for the M PowerPact circuit breaker include:
M800S - NEMA Type 1
M800R - NEMA Type 3R
M800DS - NEMA Type 4/4X/5. Type 304 Stainless Steel
M800SS - NEMA Type 4/4X/5 Type 316 Stainless Steel
M800AWK - NEMA Type 12/3R
Released for: Schneider Electric Canada