Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there an available assembled control station with 9001K15 Emergency Break-Glass operator?
Issue:
What is the part number of the complete control station with 9001K15 in it?

Product Line:
9001KY/SKY Control Stations

Environment:
Push Buttons and Operator Interface

Resolution:
Two complete units or control stations are available. Either a 9001KYK116 (with grey enclosure) or the 9001KYK117 (with red enclosure).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings