Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When ordering a factory modification form for the 8941 Duplex Controller, does it provide the option for both starters?
Issue:
Do the factory modification forms for the 8941 Duplex Controllers apply for both starters?

Product Line:
Duplex AC Motor Controllers

Environment:
NEMA Contactors and Starters

Resolution:
Only if the forms are the ones listed on page 16-96 of Digest 177. Any other forms will require the use of the form letter twice.
For example; to obtain hand-off-auto (Form C) use the form as C but if the modification is for a green off pilot light the P2 form would be required to appear twice like P2P2.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings