Browse FAQs

What is the difference between the DF6AB10 and the GK1DF fuse holders?

Published date: 14 May 2019

Issue:
What are the differences between these products? 

Product Line:
Telemecanique Fuse holders

Environment:
Products sold in North America 

Resolution:
The DF6AB10 is a 32A single-pole fuse holder.
The GK1DF is a 32A three-pole fuse holder.
Both are rated for voltages up to 500V ac and use a Class CC fuse.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.