{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What size enclosure knockouts are provided with the Class 2510 Manual Starters?

Issue:
What size enclosure knockouts are provided with the Class 2510 Type FW**, Type FR*, Type KR* and Type KW**  manual devices?

Product Line:
NEMA Contactors & Starters

Environment:
2510 Type FW, Type FR*, Type KR* and Type KW**

Resolution:
The NEMA 3R, 7 &9 and NEMA 4 enclosure are provided with (1) 3/4`` inch pipe tap located in the bottom center. These units can also be provided with (1) 3/4`` pipe tap in the top center by adding factory modification form ``H`` (i.e 2510KW1H, 2510KW1AH, 2510KR1H, 2510KR2H). Hence, there are no knockouts.

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.