{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What is wiring accessory to adapt a new Tesys contactor to existing wiring?

Issue:
Wiring accessory to adapt a new Tesys contactor to existing application.

Product Line:
TeSys™ D Contactors and Overload Relays

Environment:
Contactors and Overload Relays

Resolution:
Use an LAD4BB (which is without any coil suppression ), LAD4BBVE ( for24-48vac with suppression ), LAD4BBVG ( for 50-127vac with suppression ) or a LAD4BBVU ( for 110-250vac with suppression ). This can be used a LC1D09 to LC1D38 and LC1DT20 to LC1DT60. One of these adapters is also needed to use the LA4D electronic timers and interface modules.

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.