Browse FAQs

What is the standard lug kit for use with an I-Line style 1200 amp maximum R frame Powerpact breaker that will accept 4-#3/0 AWG to 600 KCMIL?

Published date: 24 April 2019

Issue:
Standard mechanical lug for PowerPact R.

Product Line:
Circuit Breakers
PowerPact R

Environment:
Electrical Distribution Equipment

Cause:
Replacement mechanical lug.

Resolution:
The catalog number of the replacement lug is AL1200R53K and it has 1 lug per kit.

The standard lug will accepts (4) -#3/0 AWG to 600kcmil per phase.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.