Browse FAQs

What is the replacement part number for the elapsed time meter supplied with Form G97?

Published date: 29 April 2019

Issue:
Is there an hour  or elapsed meter to check the duration of the run time for 8536 Starters?

Product Line:
NEMA Contactors &  Starters 

Environment:
Enclosure and Metering Options

Resolution:
52902-018-56 is Redington Model 722-0004.

Note: These part numbers are for replacement purposes only as not all enclosure have room to accept field installation. Elapsed time meter is rated NEMA 1 & 12 only.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.