Browse FAQs

How do you wire the Undervoltage Relay in a PowerPact H circuit breaker?

Published date: 30 April 2019

Product Line:

Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:

Connect the control wires of proper voltage to the UVR terminals under the accessory cover. Route the wires out the top of the cover through knock-outs.

Constant voltage at the correct level for the device (24V, 120V, AC, DC, etc) should be applied to terminals numbered D1 and D4. Designation for UV trip is MN.

Link to instruction bulletin 48940-22-01

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.