Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the catalog number for a 9001KM light module that can be used with any voltage lamp?
Issue:
Is there any light module base that will accept any voltage lamp?

Product Line:
9001K / 9001SK Operators

Environment:
North American Products

Resolution:
A 9001KM40 full voltage light module can be used with any voltage lamp and it is a true direct supply light module. , however, we do not supply the lamp.
Note: There are no resistors in it to drop the voltage, so it can be used with any voltage lamp up to 120 volts. Highter voltage lamps are not recommended due to heat, the lens will melt.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings