Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is a QOCRBGK1 or HOMCRBGK1?
Issue:
product design features

Product Line:
QO and Homeline load centers

Resolution:
These are the new generator interlock kits introduced to provide back-up power for indoor & outdoor, single phase, QO & Homeline load centers using QOM1 main breakers, 60 through 125 A. This generator kit interlocks the main circuit breaker with a 2 pole branch circuit breaker from 15 to 125 A.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings