{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there an offer for Nema 4X rated drives?

Issue:
Wondering if the ATV61 or ATV71 drives are available in type 4 or 4X enclosures

Product Line:
Altivar ATV61 and ATV71 open type drives

Environment:
All

Cause:
Needs to get the ATV61 and ATV71 drive in a NEMA 4 or 4X stand alone enclosure.

Resolution:
There is not a standard offering for type 4 or 4X enclosures for our drives.
It may be possible to install the drive in a properly selected enclosure by a local panel builder or contractor.
Or, contact a local SquareD field office for assistance. They may be able to offer assistance with other options.

Schneider Electric Canada

Explore more
Range:
Altivar 71Altivar 61
Explore more
Range:
Altivar 71Altivar 61
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.