Browse FAQs

What is the Terminal Lug Data for a CHU364,CH364, Series F05 Heavy Duty safety switch?

Published date: 29 April 2019

The lugs on this device will accept (1) #6 AWG - 300 kcmil aluminum or copper conductors per phase. However, wire bending space available in the switch restricts the conductors to (1) 250 kcmil maximum.


CTA-ID : 2037578

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.