Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the catalog number for the handle padlock attachment for an LA, LH, or Q4 breaker?

Article available in these languages: Spanish

Issue:
What is the catalog number for the handle padlock attachment for an LA, LH, or Q4 breaker?

Product Line:
Legacy Circuit Breakers

Resolution:
The padlock attachment is HPALM if the breaker does not have a handle extension or HPAXLM if the breaker does have a handle extension. These padlock attachments can be used to lock the breaker in the ON or the OFF position.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings