Issue:
Unable to purchase 31155-400-06
Product Line:
NEMA Contactors and Starters
Environment:
Panelboard Lighting Contactors
Resolution:
The 31155-400-06 is a restricted sub-assembly part number used in the production of the replacement coil kit. It is available only in the Class 9998 Type PBV02 coil kit for Class 8903 Type PB (panelboard) lighting contactors using 120VAC coils. The complete Class 9998 Type PBV02 coil kit also includes the full-wave bridge rectifier (31155-025-01) which supplies the coil assembly with DC power.
Unable to purchase 31155-400-06
Product Line:
NEMA Contactors and Starters
Environment:
Panelboard Lighting Contactors
Resolution:
The 31155-400-06 is a restricted sub-assembly part number used in the production of the replacement coil kit. It is available only in the Class 9998 Type PBV02 coil kit for Class 8903 Type PB (panelboard) lighting contactors using 120VAC coils. The complete Class 9998 Type PBV02 coil kit also includes the full-wave bridge rectifier (31155-025-01) which supplies the coil assembly with DC power.
Released for:Schneider Electric Canada