Browse FAQs

What is the Proper Direction the DG4/5 EPROM should face?

Published date: 16 May 2019

Issue: Installing the EEPROM on a DG5 board
 
Product line: DG5
 
Environment: Data Center Cooling
 
Cause:
 
Resolution:
NOTE THAT THERE ARE TWO STYLES OF BOARDS.
The board in your system may be one of two styles. The early style has a RED LED. The EPROM is installed on this style with the notch towards the edge of the board. The later style has a YELLOW LED. The EPROM is installed on this style with the notch away from the edge of the board and in toward the center of the board.

Do Not Use the EPROM label as a reference. Failure to install the EPROM the correct way will destroy the EPROM and may damage the interface board.

Do not install a DataGuard 5 EPROM on a board with a RED LED

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.