Browse FAQs

What is the ampere range of the PowerPact Q frame circuit breaker?

Published date: 08 May 2019

Issue:
What are the available ampere ratings on the PowerPact Q frame breakers?

Product Line:
Powerpact Circuit Breaker

Environment:
Powerpact Q-Frame

Resolution:
The PowerPact Q frame is available from 70A to 250A 2 and 3 pole. It is available as unit mount and I-Line. Unit mount versions can have lugs on both ends (L) or no lugs on either end (F) or lugs on the ON end and studs on the OFF end (M) or lugs on the OFF end and studs on the ON end (P).
Lugs can not be replaced or added on the PowerPact Q frame and no accessories are available for the PowerPact Q frame.

Note: I-Line  PowerPact Q frame is ONLY available from 70A to 225A.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.