Browse FAQs

What causes an INF3 internal serial link fault on the ATV61 and ATV71 drives?

Published date: 08 May 2020

Issue:
Getting an INF3 internal serial link fault on the ATV61 and ATV71 drives.

Product Line:
Altivar ATV61 and ATV71

Environment:
All models, all serial numbers

Cause:
Communication fault between the internal cards   

Resolution:
Check options 1 and options 2 in the Identifications menu. Check to see if there is an error reading the option cards.
Check the internal connections. Check for loose or improperly seated connections and connectors.
Inspect/repair the drive.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.