Browse FAQs

How to set the analog output assignment to motor current for an ATV61 or ATV71?

Published date: 28 February 2020

Issue: 
Set up the analog output for motor current on an ATV61 or ATV71.

Product Line:
ATV61 and ATV71

Environment:
All models

Cause:
To have an analog output signal referencing the motor current. 

Resolution:
Go to Drive Menu 1.5 Inputs/Outputs CFG AO1 Configuration
Enter on AO1 Assignment and select I motor (OCr).
Confirm the AO1 Type, AO1 min Output, AO1 max Output and Scaling AO1 match the analog output signal expected.  The default selection is 0 - 20mA for amp range 0 - 2 x In (In = rated drive current indicated on VFD nameplate).


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.