Browse FAQs

What is the adapter part number to connect a Quantum with a RJ45 serial port to a TSXCUSB232?

Published date: 31 May 2019

Issue:
Adapter part number to connect a Quantum with a RJ45 serial port to a TSXCUSB232

Product line:
High end Quantum's, all Momentums, and all Compact 984 with RJ45 connectors 

Cause:
Cable parts to be able to connect to the RJ45 ports on PLC's

Resolution:
The part number for the adapter is 110XCA20300 and the 110XCA28202.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.