Browse FAQs

Are the MA-0185-100 Taps compatible with the MA-0185-000 Taps?

Published date: 30 April 2019

Yes, the MA-0185-100 Tap are only compatible with the MA-0185-000 Revision C or higher Taps. If you have the MA-0185-000 lower than the revision C, MA-0185-100 is not compatible. You would need to either find another MA-0185-000 below the Rev C or replace all the Taps on the network to the MA-0185-100.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.