{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}
Goals and Symptoms
In the project settings of UnityPro you can activate for SFC multiple token. In this case you can also define the maximum number of active steps. If you have more active steps in your project as defined in the project settings the simulator goes into ERROR state at the end of the project transfer.
Causes and Fixes
Increase the number of active steps for multiple token in the project settings. No correction of UnityPro simulator is planned, because of the high effort to change the error handling of the simulator allmost completely.