Browse FAQs

What are the default OTB1S0MD9LP Modbus port setting and can they be changed?

Published date: 13 May 2019

Issue:
How to change the Port setting  on a Modbus OTB.

Product line:
Advantys OTB serial 

Environment:
Advantys configuration software

Cause:
Unable to change the port setting on the Modbus OTB

Resolution:
The default parameters for the OTB1S0DM9LP are as follows;
MODE: RTU
PARITY: EVEN
STOP BIT: 1
DATA BIT: 8

The above parameters are fixed and can not be changed. The only thing that can be changed is the BAUD RATE and ADDRESS and this is done with the rotary switches on the module.


Note: The OTB TM2 modules will be obsolete 9/1/2018 and it would be recommended to look for a replacement either the STB product line or the M221 line as a replacement.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.