Browse FAQs

Can the Quantum 140CPU11303 be programmed in both IEC and 984LL using Concept?

Published date: 19 April 2019

Issue:
Capability of having 984 LL or IEC program loaded into the 11303 Quantum processor.

Product line:
Quantum

Environment:
Concept software

Resolution:
Yes. The 140CPU11303 will support a hybrid application including both 984LL or IEC depending on the exec firmware loaded into the controller.
This would not be possible with the 140CPU11302 processor due to its limited memory.

NOTE: The Quantum processors are obsolete and the recommended replacement would be the M580 and the I/O can stay in place or be upgraded to the x80 I/O and Unity Pro will concert the program to the M580. For more information on this contact your local distributor.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.