Browse FAQs

What is the difference between Save Project, Backup Project and Restore Project in the ProWORX 32 programming software?

Published date: 30 April 2019

Issue
Difference between Save, Backup, and Restore project

Product Line
ProWORX 32

Resolution
SAVE PROJECT saves the current project you're working on. This will be the .PWX file.
BACKUP PROJECT saves a backup copy of the project you're working on. ProWORX 32 will create a .BAK file of the backed up project. This way you can always go back and Restore a Backed Up project if it's been saved as a .BAK file.

RESTORE PROJECT in ProWORX 32 is used if you want to restore a current project back to an older version of the same project that has been backed up.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.