Browse FAQs

Is there an example on how to program a "Flasher Circuit" using 984 Ladder Logic that can be used as an annunciator?

Published date: 30 April 2019

Issue
Flasher Circuit programming in 984 Lader Logic

Product Line
EcoStruxure Control Expert
Concept 
Proworx

Enviroment
LL984

Resolution
Below is a 984 Ladder Logic example of a "Flasher Circuit". The first Timer is the "Off" time and the second Timer is the "On" time. The example is a 1 second "Off" and 1 second "On" for output 00001..


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.