Browse FAQs

Does the ETL / EGX300 logging tool work with ION Enterprise and StruxureWare Power Monitoring?

Published date: 17 May 2019

Issue
Does the ETL / EGX300 logging tool work with ION Enterprise, StruxureWare Power Monitoring and Power Monitoring Expert?

Product Line
IONE, SPM  and PME

Environment
Power Monitoring Software

Cause
Need to know if the ETL/EGX300 logging works with IONE, SPM and PME

Resolution
The EGX300 ETL package works with the following versions:

  • ION:E 6.0 or 6.0 sp1 (Note that ETL tool is not free with ION Enterprise 6.0 or 6.0 SP1.
  • One should contact sales to purchase the right version for ION Enterprise V 6.0 SP1)
  • SPM 7 or 7.0.1 and Power Monitoring Expert (PME)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.