Browse FAQs

Are the TeSys K 3 pole reversing mini-contactors and overloads designed with provision for panel and din rail mounting capacities?

Published date: 09 May 2019

Issue:
Are the TeSys K 3 pole reversing mini-contactors and overloads designed with provision for panel and din rail mounting capacities? Is there an accessory available that provides the separate mounting of the TeSys K overload modules which positions the overload block on the same din rail track as the contactor?

Product Line:
TeSys K 3 Pole Reversing & Non-Reversing Contactors, TeSys K accessories

Environment:
TeSys K

Cause:
Assembly/wiring

Resolution:
TeSys K mini-contactors are provided with panel mounting and Din 3 (35 mm) capabilities. To separately mount the overload relay onto 35mmm din rail, use the part number LA7K0064.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.