{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What is SAFF fault on ATV32?

Issue:
What is SAFF fault on ATV32?

Product Line:
ATV32 drives

Environment:
SAFF

Cause:
n/a

Resolution:
When the following safety functions are being used on the ATV32:

- (STO) Safe Torque Off
- (SS1) Safe Stop 1
- SLS) Safely Limited Speed

You can check your drive configuration file to see if the have been assigned.

If so please refer to the Altivar 32 Variable speed drives for synchronous and asynchronous motors Safety integrated functions manual.
Explore more
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}
Explore more