Browse FAQs

When I enable the input range in my numeric display, it is set to min=0 and max=0 at runtime.

Published date: 24 April 2019

Issue:
When I enable the input range in my numeric display, it is set to min=0 and max=0 at runtime.

Product Line:
Vijeo Designer (all versions)

Resolution:
This issue occurs when you have a mismatch between the variable Data Type and the Numeric Display Data Type. For example, if your variable is INT and your Numeric Display is for "FLOAT", the input range will not work correctly. The data types must be the same. For INT use Integer. For REAL, use FLOAT.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.