Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unable to select an "End date" for the database archive when "Beginning of the database" is selected using Database Manager

Issue
The "End date" is greyed out in the Database Manager when "Beginning of the database" is selected during an archive database configuration

Product
Power Monitoring Expert 8.1

Environment
Database Archiving

Cause
This behavior became apparent with the release of Power Monitoring Expert (PME) 8.1.

Note: The behavior was changed and subsequent releases (PME 8.2 and PME 9.0) do not require the workaround explained below.

Resolution
Use the following workaround:

  1. Instead of selecting beginning of the database, select a date range
  2. The start day can be any day before the beginning of the database. For example, if it is known that the system was commission in June of 2015, The start date can be set to May of 2015 or any earlier date
  3. Once, the date is selected make sure that the "Remove Archive data from the live database" is marked accordingly. If the data needs to be removed from the database make sure this is checked.




Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings