Browse FAQs

Does the SR2MOD03 wireless modem support 3G networks?

Published date: 08 May 2019

Issue:
Does the SR2MOD03 wireless modem work with 3G networks?

Product Line:
SR2MOD03

Resolution:
The modems with manufacturing dates greater than or equal to 1630 support 3G and are six Bands (Band I (2100 MHz), Band II (1900 MHz), Band IV (1700 MHz), Band V (850 MHz), Band VI (800 MHz) and Band VIII (900 MHz)) in 3G UMTS/HSDPA/HSUPA.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.